FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > FR-PA07
FAQ
FR-PA07
Is the mounting screw supplied with the optional FR-PA07?
Do I have to use a nut for the installation?
Do I have to use a nut for the installation?
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
The mounting screw is not supplied. The mounting screw is supplied with the operation panel.
Open the screw hole according to the dimension. (The M3 screw is used.)
Open the screw hole according to the dimension. (The M3 screw is used.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700