Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21363
  • Release Date : 2018/08/22 16:27
  • Print

FR-PA07

When using the enclosure surface operation panel FR-PA07, is there any necessary settings?
Category : 

Answer

Specific settings are not required, however, when replacing the FR-E500, check that Pr.146 (Built-in potentiometer switchover) is not set to "0".
If it is "0", change it to "1".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries