Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21416
  • Release Date : 2018/08/22 16:27
  • Print

Frequency setting

How can I set the inverter frequency to 120 Hz using the potentiometer of the FR-E520?
Category : 

Answer

Ensure that the inverter is in the PU operation mode and stopped, change the following parameters:
1. Read Pr.923 (Built-in frequency setting potentiometer gain).
2. Change it to 120 Hz, and press and hold the SET key for 1.5 seconds.
3. Turn the built-in potentiometer to the rightmost position.
4. Press and hold the SET key for 1.5 seconds again.
Setting is complete when the display blinks.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries