FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Coasting
FAQ
Coasting
The output is shut off in the shortest time when Pr.250 is set to "0". When the output is stopped by inverter contact input, is the value set by Pr.250 referenced?
- Category :
Answer
When the inverter output shutoff signal MRS is turned on, the output is shut off immediately without regard to setting of Pr.250.
- Product Name
- Inverter, magnet motor drive
- Series
- FR-A500