Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21431
  • Release Date : 2018/08/22 16:27
  • Print

Inverter data cannot be read

I want to use the inverter configuration software "FR-SW0-SETUP-WJ" to read the inverter data, but an error message "Inverter not connected" appears upon completion of data reading (100%) and data cannot be read.
Performing "Data display" after that causes an error and the process terminates.
What are the possible causes for this?
Category : 

Answer

It is considered that communication settings between the inverter and personal computer do not match.
Check if settings such as communication rate and stop bits match between them.
Note that initial setting of Pr.122 (Communication check time interval) does not allow for correct communication with the personal computer. Also, check this parameter setting.
Product Name
Inverter, magnet motor drive
Product Category
Inverter setup software
Series
Engineering software

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries