Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21453
  • Release Date : 2018/08/22 16:27
  • Print

Output current detection

I am planning to choose the FR-A240E.
I want to detect the state where the actual output current higher than the set value flows to detect motor signal loss, and input the detection signal to the programmable controller.
Can I do this with the FR-A240E?
Category : 

Answer

The FR-A500 series that is the successor of the FR-A200E series has a function similar to output current detection of the FR-E500.
Consider using the FR-A500 series.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A200, FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries