Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21464
  • Release Date : 2018/08/22 16:27
  • Print

Connecting voltmeter to terminal AM

I am considering to connect two voltmeters (YM-8DV) to the terminal AM of the FR-A540-0.4K.
Can I connect them in parallel?
Category : 

Answer

You can connect them in parallel.
Connect the voltmeters in parallel, paying attention to the following:

- The output current should not exceed the permissible value of 1 mA when the output voltage of the terminal AM (maximum output) is 10 V.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries