FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Support of Chinese
FAQ
Support of Chinese
I received inquiry for exporting to China via a set manufacturer. One of the conditions is "Manuals written in Chinese should be available". Do you have manuals written in Chinese?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > Others
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
Answer
Some types are designed for the Chinese market and provide Chinese manuals. (Note that the specifications of these types are partially different from the specifications for the Japanese market, there is no manual of the Japanese specifications products translated into Chinese.) The Chinese specifications products can be purchased in Japan. Contact your distributors or local office.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-E700, FR-D700, FR-A700, FR-F700