FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > What is the replacement of the FR-BOL?
FAQ
What is the replacement of the FR-BOL?
I have the FR-Z100 series inverter used in the existing system. If I replace it with the FR-A100E series, what is the replacement for the FR-BOL?
- Category :
Answer
We do not offer a replacement product for the FR-BOL (noise reduction reactor). Since the FR-A100E is a low-noise type inverter, the motor noise is suppressed and you do not need the FR-BOL. Note that, since the FR-A100E uses high carrier frequency sine wave PWM control, noise and leakage current increase compared to the FR-Z100. If noise or leakage current occurs, lower the carrier frequency (Pr.72) to the same level as the FR-Z100 (approximately 1 kHz) and use the FR-BOL. Also, refer to our noise data sample. Figure 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- Option