Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21512
  • Release Date : 2018/08/22 16:28
  • Print

A100 inverter loss

Before delivering the 3.7 to 7.5K inverters, economy analysis is requested.
The A100 technical material provides heat generation data and the total load efficiency for the 3.7 to 7.5K class is 95% or less. Can I use these values for analysis?
How much is the loss of the controller part including the fan?
Category : 

Answer

The inverter efficiency (power factor) for the inverter alone is approximately 75 to 80%.
However, by installing the power factor improving DC reactor to the inverter, the power factor increases to 95%.

Also, the heat generation quantity with only the inverter power supply turned ON is approximately 25% of the heat generation quantity for the inverter rated output current, due to power supply to the fan and power consumption inside the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries