Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21521
  • Release Date : 2018/08/22 16:28
  • Print

FR-E520 7.5 kW model

What are the outline dimensions of the above model? This model is not listed on your catalog.
Currently, I use the FR-A520 as the 7.5 kW inverter.
If the FR-E520 is smaller and less expensive, I want to adopt it.
Category : 

Answer

The outline dimensions of the FR-E520-7.5K are 180W×260H×170D.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries