Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21532
  • Release Date : 2018/08/22 16:28
  • Print

Parameters not covered in manual are displayed

On the FR-E520-0.4K, 0.75K, and 2.2K inverters, No.168 and No.169 that are not covered in the manual are displayed.
Pr.168 is set to "7362" and Pr.169 is set to "5". What are these parameters?
Category : 

Answer

Pr.168 indicates the inverter software version.
Pr.169 indicates the inverter software subversion history.

These two parameters are only used by the manufacturer to determine the software version.
Therefore, there are read-only and cannot be changed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries