FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Connecting operation panel to enclosure
FAQ
Connecting operation panel to enclosure
Which cable should I use to connect the operation panel to the enclosure?
What is the maximum cable length in this case?
What is the maximum cable length in this case?
- Category :
Answer
To connect the operation panel to the enclosure, use the parameter unit connection cable FR-CB201, FR-CB203, or FR-CB205. The maximum cable length is 5 m.
Note that you need the control panel rear cover and adapter set to connect the operation panel to the enclosure.
Note that you need the control panel rear cover and adapter set to connect the operation panel to the enclosure.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500