Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21547
  • Release Date : 2018/08/22 16:28
  • Print

Sensitivity current of earth leakage circuit breaker

The earth leakage circuit breaker NV-FA series is available for the sensitivity current 30 mA only. Can I install it on the inverter input side?
Category : 

Answer

The rated sensitivity current of the earth leakage circuit breaker can be calculated using the following equation.
If the result is 30 mA or less, the NV-FA series can be used.
(If not, you need to use a NV type with a higher rated sensitivity current.)
Product Name
Inverter, magnet motor drive
Product Category
Earth leakage circuit breaker
Series
Peripheral devices

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries