FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Size
FAQ
Size
How large is it?
- Category :
Answer
The high power factor converter itself is almost same size as general-purpose inverter with the same capacity (FREQROL-A200 series), however, an additional space to install accessories (outside box, reactor 1, and reactor 2) is required.
The ratio between the installation spaces for the converter and accessories is approximately 1:1.5.
The ratio between the installation spaces for the converter and accessories is approximately 1:1.5.
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option