FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > SC-A > Can I input speed setting externally with the box type?
FAQ
Can I input speed setting externally with the box type?
Can I input speed setting externally with the box type?
- Category :
Answer
No.
Use the potentiometer on the box to set the speed. If you want to input analog values externally to set the speed, use the unit (module) type.
Use the potentiometer on the box to set the speed. If you want to input analog values externally to set the speed, use the unit (module) type.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A