FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A024 > Do noise and leakage current increase?
FAQ
Do noise and leakage current increase?
Do noise and leakage current increase compared to the conventional FR-Z024?
- Category :
Answer
During non-low-noise operation (initial setting) with the carrier frequency of 1 kHz, both noise and leakage current levels are almost same as the Z024 series.
Note that noise and leakage current increase during low-noise operation with higher carrier frequency.
You can change the carrier frequency by Pr.72 (PWM frequency selection). (The initial setting is 1 kHz.)
Note that noise and leakage current increase during low-noise operation with higher carrier frequency.
You can change the carrier frequency by Pr.72 (PWM frequency selection). (The initial setting is 1 kHz.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024