Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21606
  • Release Date : 2018/08/22 16:28
  • Print

Do noise and leakage current increase?

Do noise and leakage current increase compared to the conventional FR-Z024?
Category : 

Answer

During non-low-noise operation (initial setting) with the carrier frequency of 1 kHz, both noise and leakage current levels are almost same as the Z024 series.
Note that noise and leakage current increase during low-noise operation with higher carrier frequency.
You can change the carrier frequency by Pr.72 (PWM frequency selection). (The initial setting is 1 kHz.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries