Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21611
  • Release Date : 2018/08/22 16:28
  • Print

Can I use it with the single-phase power supply?

Can I use it with the single-phase power supply?
Category : 

Answer

You can use the inverter with the single-phase 200 V power supply. However, since ripple current flowing through the capacitor increases and the converter and capacitor temperature goes high, you need to reduce the output rating to half.
Be sure to connect to the power supply side terminals R and S. (It cannot be used with single-phase 100 V power supply.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries