FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A024 > How many inverters can I connect using the communication unit?
FAQ
How many inverters can I connect using the communication unit?
How many inverters can I connect when the communication unit (FR-CU01 or FR-CU03) is used?
- Category :
Answer
Since the communication unit conforms to the EIA Standard RS-485, up to 32 inverters can be connected. (Transmission format: Multidrop link, total wiring length: 500 m)(Note) Use the connection cable FR-CBL when using the FR-CU01.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024