Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21617
  • Release Date : 2018/08/22 16:28
  • Print

Installation of new serial communication unit FR-CU03

Where should I install the new serial communication unit FR-CU03?
Category : 

Answer

Remove the parameter unit FR-PU03 and install there. (The installation dimensions of the FR-CU03 are the same as the FR-PU.)
You can read and write parameters as well as start and stop the inverter via the communication cable from a personal computer.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries