Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21618
  • Release Date : 2018/08/22 16:28
  • Print

How much low-speed torque can be output?

How much low-speed torque can be output?
Category : 

Answer

By choosing the General-purpose magnetic flux vector control and slip compensation function, you can output torque of 150% or more at 1 Hz (200% or more at 3 Hz). (Maximum short-time torque)(For the Mitsubishi standard motor 4P)
For the Mitsubishi standard motor 0.4 to 1.5 kW 4P, continuous 100% torque operation at 6 to 60 Hz is possible in combination with General-purpose magnetic flux vector control.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A024

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries