Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21623
  • Release Date : 2018/08/22 16:28
  • Print

Comparison of noise between FR-A100 and FR-A100E

Does the FR-A100E produce noise less than the FR-A100?
Category : 

Answer

The setting ranges of the carrier frequency are:
- FR-A100: 2 kHz to 14.5 kHz
- FR-A100EXCELLENT: 0.7 kHz to 14.5 kHz
The range of the FR-A100EXCELLENT is extended to the lower side, meaning that you can set the carrier frequency lower than the FR-A100. This means that noise can be reduced more than the FR-A100.

For the same carrier frequency, the noise levels are almost same.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries