FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Connecting high power factor converter
FAQ
Connecting high power factor converter
Can I connect it to the high power factor converter FR-HC?
- Category :
Answer
You can connect the high power factor converter to an inverter if the inverter supports it.
The conventional inverters do not have the high power factor converter connection parameters and you cannot connect the converter to them.
Be sure to connect the converter to a compatible inverter.
The conventional inverters do not have the high power factor converter connection parameters and you cannot connect the converter to them.
Be sure to connect the converter to a compatible inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200