FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A200 > Compatibility of the function with FR-A200
FAQ
Compatibility of the function with FR-A200
Are the functions of the FR-A200EXCELLENT and FR-A200 compatible?
- Category :
Answer
Yes.
Compared with the FR-A200:
- The auto tuning function is added.
- Response current limit operation is improved.
- The carrier frequency range is extended.
(Note)The FR-APA to APE options for the FR-A200 cannot be used with the FR-A200EXCELLENT.
Use the dedicated options FR-EPA to EPE, EPG, and EPH.
Compared with the FR-A200:
- The auto tuning function is added.
- Response current limit operation is improved.
- The carrier frequency range is extended.
(Note)The FR-APA to APE options for the FR-A200 cannot be used with the FR-A200EXCELLENT.
Use the dedicated options FR-EPA to EPE, EPG, and EPH.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200