Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21631
  • Release Date : 2018/08/22 16:28
  • Print

Compatibility of the installation between FR-A200EXCELLENT and FR-A200?

Are the FR-A200EXCELLENT and FR-A200 compatible in installation?
Category : 

Answer

Yes. (However, since they are aligned with the small size of the FR-A200 (D), you need to use the intercompatibility attachment FR-AAT for a larger size.
Attaching this attachment to the inverter increases the depth of the inverter for 12 to 15 mm.

The following four types require the attachment:          
FR-AAT-02 for FR-A220-11K
FR-AAT-10 for FR-A220-45K
FR-AAT-09 for FR-A240-30K
FR-AAT-10 for FR-A240-45K
(The FR-A220D-11K does not require the attachment.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries