FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A200 > Plug-in options
FAQ
Plug-in options
Can I use the plug-in option used with the FR-A200 with the FR-A200EXCELLENT?
- Category :
Answer
Use the plug-in option dedicated for the FR-A200EXECLLENT.
The plug-in option for the FR-A200EXECLLENT cannot be used with the FR-A200.
To avoid installing an incorrect plug-in option, the connector position of the option for the FR-A200EXCELLENT is different from the option for the FR-A200.
Do not install an incorrect option forcibly because doing so breaks the plug-in option unit.
The functions of the FR-EPA to FR-EPE are the same as those of the conventional FR-A200 options (FR-APA to FR-APE).
For the FR-A200EXCELLENT, the FR-EPG and FR-EPH options are added.
The plug-in option for the FR-A200EXECLLENT cannot be used with the FR-A200.
To avoid installing an incorrect plug-in option, the connector position of the option for the FR-A200EXCELLENT is different from the option for the FR-A200.
Do not install an incorrect option forcibly because doing so breaks the plug-in option unit.
The functions of the FR-EPA to FR-EPE are the same as those of the conventional FR-A200 options (FR-APA to FR-APE).
For the FR-A200EXCELLENT, the FR-EPG and FR-EPH options are added.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-A200