Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21635
  • Release Date : 2018/08/22 16:28
  • Print

Difference from FREQROL-A200 (EXCELLENT) series

What are the differences from the FREQROL-A200 (EXCELLENT)?
Category : 

Answer

The following features are added to the FREQROL-A200 (EXCELLENT):
- PI control without an option
- Inverter electronic bypass sequenceThe following functions of the FREQROL-A200 (EXCELLENT) are not provided:
- Magnetic flux vector control
- Auto tuning
- Intelligent mode (shortest acceleration/deceleration, lift)
- Regenerative brake resistor (external installation is also not allowed)
- FR-EPA option installation
The permissible overload is reduced from the FREQROL-A200 (EXCELLENT). The size is reduced by one rank except for some capacities. The size is reduced by one rank except for some capacities.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries