Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21638
  • Release Date : 2018/08/22 16:28
  • Print

What functions are added compared with FR-A200?

What functions are added to the FR-A200EXCELLENT compared with the FR-A200?
Category : 

Answer

The following functions are added or improved:
- Auto tuning function- Fast-response current limit operation is improved.- Characteristics of magnetic flux vector control is improved.- The carrier frequency setting range is extended.- Communication speed of plug-in option is improved.And others.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries