Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21653
  • Release Date : 2018/08/22 16:28
  • Print

Applicable motors

What types of motors are applicable?
Category : 

Answer

In addition to the dedicated motor (SF-VR series), the SF-JR series motor with an encoder can be used.
You can also use a standard motor by combining it with an encoder.
Further, you can use a geared motor by combining it with an encoder and performing auto tuning.
Note that the encoder must be directly linked to the motor shaft.
You can use motors with encoders from other manufacturers by performing auto tuning.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries