Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21665
  • Release Date : 2018/08/22 16:28
  • Print

FR-BU2

Can I use the brake unit FR-BU2 with the FR-E740-1.5K?
The motor capacity is 1.5 kW.
Category : 

Answer

You cannot use the brake unit FR-BU2 with the FR-E740-1.5K.

To use the brake unit, increase the inverter capacity to 2.2K.

You can use the brake unit with the FR-BU2-H7.5K and six discharging resistors GRZG200-10Ω connected in series.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries