FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Cooling fan
FAQ
Cooling fan
Does the cooling fan operate just by powering on the inverter?
Pr.244 (Cooling fan operation selection) is not changed from the initial value.
Pr.244 (Cooling fan operation selection) is not changed from the initial value.
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
Pr.244 (Cooling fan operation selection) controls turning ON/OFF of the cooling fan and is initially set to "1". When the inverter is powered ON, the cooling fan operates if the internal temperature of the inverter is high. It does not operate if the temperature is low.
While inverter running, the cooling fan operates regardless of the internal temperature.
While inverter running, the cooling fan operates regardless of the internal temperature.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700