Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21672
  • Release Date : 2018/08/22 16:28
  • Print

Full scale frequency

A full-scale 1 mA DC analog meter is connected between the terminals FM and SD. Can I change the full-scale frequency?
Category : 

Answer

You can change the full-scale value by changing Pr.55 (Frequency monitor reference).

The initial setting is 60 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries