FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Terminal
FAQ
Terminal
I want to use the inverter terminal 4 to operate the inverter at 85 Hz when 20 mA is input from the current 4 to 20 mA input.
Should I change the setting of Pr.125 (Terminal 2 frequency setting gain frequency)?
Should I change the setting of Pr.125 (Terminal 2 frequency setting gain frequency)?
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
Change Pr.126 (Terminal 4 frequency setting gain frequency).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700