FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Terminal
FAQ
Terminal
Must I turn ON the terminal AU to use the inverter terminal 4?
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
Signals input from the terminal 4 are not enabled if the terminal AU is not ON.
For an inverter without the terminal AU, assign the AU function to an unused terminal and turn it ON.
For the E700 series, for example, if the terminal MRS is unused, changing Pr.183 to "4" changes the function of the terminal MRS to AU.
For an inverter without the terminal AU, assign the AU function to an unused terminal and turn it ON.
For the E700 series, for example, if the terminal MRS is unused, changing Pr.183 to "4" changes the function of the terminal MRS to AU.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700