FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Output frequency
FAQ
Output frequency
I want to input the inverter output frequency to the analog unit of the programmable controller to control other devices.
I want to receive it as 4 to 20 mA DC.
How can I do this?
I want to receive it as 4 to 20 mA DC.
How can I do this?
- Category :
Answer
For the FR-E700, only the terminal FM allows for variable output and the output is a pulse signal. Therefore, it cannot be directly input to the programmable controller. For your purpose, use another device as followings:(1) Convert the output pulse into 4 to 20 mA using a pulse converter.
(2) Take 0 to 20 mA output from the terminal AM1 of the plug-in option FR-A7AY.
(2) Take 0 to 20 mA output from the terminal AM1 of the plug-in option FR-A7AY.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700