Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21685
  • Release Date : 2018/08/22 16:28
  • Print

Frequency setting

I want to apply analog voltage to the inverter terminal 2, and use 0 to 5 VDC input to set the frequency to 20 Hz to 60 Hz.
How should I configure the setting?
Category : 

Answer

Adjust the terminal 2 bias with Pr.C2 and Pr.C3, and the terminal 2 gain with Pr.125 and Pr.C4.
Set Pr.C2 (Terminal 2 frequency setting bias frequency) to 20 Hz and Pr.125 (Terminal 2 frequency setting gain frequency) to 60 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries