FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Adjustment of analog gain
FAQ
Adjustment of analog gain
I input analog signals from the terminal 2. When I tried to adjust the analog gain, I could not find Pr.903 (Frequency setting voltage gain) that was found with the FR-E500.
How can I find this parameter?
How can I find this parameter?
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
Use Pr.903 (Frequency setting voltage gain) for setting the FR-E500. For the 700 series, use Pr.125 (Terminal 2 frequency setting gain frequency) and Pr.C4 (Terminal 2 frequency setting gain) for calibration.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700