FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > RUN blinks
FAQ
RUN blinks
RUN blinks and operation does not start. I enter an external startup signal to start operation and use the setting dial to set the frequency. The running frequency is set to 24 Hz.
The operation mode Pr.79 is set to "3"
The operation mode Pr.79 is set to "3"
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
When using the setting dial to set the frequency, turn the dial and press the "SET" key while the desired value flickers. (The value and "F" flicker alternately). The frequency setting is completed if the value flickers. If it does not flicker, the frequency is not set and operation does not start when the startup signal is entered.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700