FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > PU operation
FAQ
PU operation
Pressing the PU/EXT button does not switch to PU. I want to change the frequency.
An external start command is used and the frequency is set with the setting dial.
PU, EXT, and MON turn ON.
An external start command is used and the frequency is set with the setting dial.
PU, EXT, and MON turn ON.
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
If Pr.79 = 3, PU and EXT turn ON. Switching between PU and EXT is not available. Turn the setting dial to set the frequency and press the SET key to accept it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700