Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21702
  • Release Date : 2018/08/22 16:29
  • Print

FR-PA07

I am using the optional operation panel FR-PA07 connected with a cable with Pr.79 (Operation mode) set to "3".
How can I switch between the setting dial and multi-speed settings?
Category : 

Answer

There is a priority between the setting dial and multi-speed settings.

Since the multi-speed setting is given a higher priority, the setting by the setting dial does not take effect unless all of the multi-speed signals are OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries