Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21705
  • Release Date : 2018/08/22 16:29
  • Print

FR-E740

What is the amount of heat generated for each of the capacities from FR-E740-0.4K to 15K?
Category : 

Answer

The following is the amount of heat generated for each capacity:

0.4K: 40W  0.75K: 55W  1.5K: 90W  2.2K: 100W

3.7K: 180W  5.5K: 240W  7.5K: 300W  11K: 400W

15K: 500W
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries