Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21711
  • Release Date : 2018/08/22 16:29
  • Print

FR-Configurator

While using the inverter's terminal 4 (for 4-20 mA) and supplying 20 mA, I want to operate it at 85 Hz.
Can I set this by using the optional setup software (FR-SW3-SETUP-WJ)?
Category : 

Answer

Yes, you can use the setup software (FR-SW3-SETUP-WJ) to set it.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries