FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Monitor indicator
FAQ
Monitor indicator
How should I set the inverter to check the rotations per minute on its monitor?
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
Set Pr.37 (Speed display) to the speed obtained when operating the machine at the frequency set with Pr.505 (Speed setting reference). (For FR-F700/E700/D700, set the speed obtained when operating the machine at 60 Hz.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700