Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21725
  • Release Date : 2018/08/22 16:29
  • Print

Electromagnetic contactor

Is it fine to turn ON/OFF the electromagnetic contactor using the push button on the output side of the inverter? 
Category : 

Answer

Turning ON/OFF the output side during operation causes open/close surges that may trigger the protective function (against overcurrent or overvoltage) of the inverter or may even cause a failure. Turn ON/OFF the output side while the inverter is not operating.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?