FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
Can I change Pr.1 (Maximum frequency) during operation?
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
No. You cannot change the setting during operation.
However, setting Pr.77 (Parameter write selection) to "2" allows for the setting change during operation. (Note that changing other parameters is also allowed.)
However, setting Pr.77 (Parameter write selection) to "2" allows for the setting change during operation. (Note that changing other parameters is also allowed.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700