Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21750
  • Release Date : 2018/08/22 16:29
  • Print

Auto tuning

When I set Pr.96 (Auto tuning setting/status) to "1", "96" and "1" flicker alternately. What should I do next?  
Category : 

Answer

If you have already set other parameters necessary for tuning (Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, and Pr.84), press the MODE button to return to the frequency monitor window.

You will notice that "1" is shown. ("1" is not shown if auto tuning is not set.)

Sending the start command after that starts auto tuning.

Indication proceeds from "1", "2", and "3", and auto tuning completes. Turn off the start command.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries