Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21764
  • Release Date : 2018/08/22 16:29
  • Print

Monitor indicator

How can I switch the monitor display from the output frequency to output current?  
Category : 

Answer

Press the "SET" key once while the output frequency is monitored.

The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries