FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter setting
FAQ
Parameter setting
I want to install a full-scale 100 Hz frequency meter.
Which parameter should I set for this purpose?
Which parameter should I set for this purpose?
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
Set Pr.55 (Frequency monitor reference) to "100 Hz".
If the indication of the installed frequency meter does not match the running frequency, use the calibration parameter Pr.C0 (FM terminal calibration) to adjust it.
If the indication of the installed frequency meter does not match the running frequency, use the calibration parameter Pr.C0 (FM terminal calibration) to adjust it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700