FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Display unit of operation panel
FAQ
Display unit of operation panel
I want to change the display unit of the operation panel from frequency to rotations per minute.
- Category :
Answer
Set the rotations per minute that is obtained while operating at the frequency set with Pr.505 (Speed setting reference) to Pr.37 (Speed display).
For example, when Pr.505 = 50 Hz and Pr.37 = 1500 and the running frequency is 50 Hz, the running speed monitor shows "1500".
However, if Pr.144 (Speed setting switchover) = 0, the display value remains as frequency.
For example, when Pr.505 = 50 Hz and Pr.37 = 1500 and the running frequency is 50 Hz, the running speed monitor shows "1500".
However, if Pr.144 (Speed setting switchover) = 0, the display value remains as frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F700PJ, FR-A700, FR-F700P